Field Visibility and Display Name

There are a few important considerations regarding Wavepoint’s access to data fields:

  • Wavepoint’s access to the underlying fiber data is only through the published service. Thus, if you turn off fields, you hamper Wavepoint’s functionality.

    In the Layer Properties dialog > Fields tab, ensure all layers are checked to be visible:


  • Wavepoint always lists fields in alphabetical order regardless of how they are sorted in ArcMap. Sorting layers in the Fields tab does not change their display order in Wavepoint.

  • Each fiber facility in Wavepoint has a display name. This is configured in the Layer Properties dialog > Display tab:


    And this choice is seen in Wavepoint:


    • You can choose one field to act as the display name field. Wavepoint does not support field expressions (for example, concatenating multiple fields) for the display name.

    • If you do not choose a display field (or if the chosen field is null), Wavepoint uses the ObjectID.


      Because this is not very helpful, we recommend choosing a relevant field that is usually populated.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.