Configure Relationships and Model Names

Because Wavepoint is published from a map service with Fiber Manager data, most of the relationships and model names covered in the subsequent topics were likely created during your Fiber Manager implementation. However, where Fiber Manager is a flexible data model, Wavepoint is not, and thus you should still confirm the relationships and model names, and configure them if they are missing.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.