Verify Map Service Configuration

Results listed on this page are mainly driven by model names that Wavepoint looks for in the published map service. Thus, the list of tables below might not exactly match the list of tables that exist in your published service. And in the Fields section, only tables that have required model names are listed, thus, that list might not exactly match the list in your published service.

  1. Open Wavepoint using the URL https://servername.domain.com:6443/Wavepoint.
  2. In the upper, right-hand corner of the browser, click the user name.
  3. The choices vary depending on your user and authentication method:
    1. If logged in using Windows authentication or if logged in as a non-administrator with Forms authentication:

    2. If logged in as an administrator with Forms authentication:

  4. Click Verify Configuration.

Understanding Results

Examine the verification results.

Result

Description

Validation was successful.

An optional configuration is not set up. The application will still work, but functionality might be missing.

Validation was unsuccessful. The application will not work properly. See below for possible fixes to these configuration problems.

The verification sections only show results for configured feature and object classes included in the published map service. After compiling the list of feature and object classes, the application then checks for the appropriate fields, relationships, and Global IDs. In other words, if your company has not configured small form-factor pluggable (SFP) transceivers, then they do not display in any of the verification results.

As an example, the following image displays condensed portions of the validation output:

The number in parentheses refer to the layer number in the published service. It does not refer to the number of records or features.

TIP: The quickest way to see the layers in the published service is to view the REST URL. To do so:
  1. In ArcGIS Server Manager, click Services.

  2. Locate your published service, then click the name of the service.

  3. Click Capabilities, then click the REST URL.

  4. Notice all the layers and tables are displayed in the service. The published order comes from the Table of Contents in the underlying map document used.

For Wavepoint to function properly, all red Xs must be corrected. Re-run the verification process to ensure issues have been resolved. Once all the Tables and Fields sections have green checkmarks, you may proceed with the next steps in the configuration.


What Might be Wrong?

Based on the location of any red Xs you see, one of the following situations is occurring:

  • Tables

    • The table is published but is not assigned the necessary class model name.

    • The same class model name is assigned to more than one of the tables (or, more likely, multiple layers possessing the same model name were published in the map service).

  • Fields
    • The field does not exist on the table.

    • The same field model name is assigned to more than one field.

  • Relationships
    • Usually problems in this portion of the test results are resolved by fixing problems that appear in the Tables portion of the report.

  • Global IDs
    • The GlobalID field for certain tables is not published.

    • The GLOBALID field model name is missing.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.