Configure IIS

If your server's firewall blocks port 6080, begin the Wavepoint installation process by running Web_Adaptor_for_Microsoft_IIS from Esri. This installer is included in the ArcGIS Server full installer package.

Then, review the next sections to ensure the computer acting as the server has the correct Windows IIS features enabled.

Some Wavepoint functionality, for example the Move to Current Location tool, depends on a secure service. Schneider Electric strongly recommends implementing Wavepoint as a secure service for full functionality. In other words, deploy as https:// and not http://.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.