Windows Server 2012 R2

  1. In the Start menu, right-click Computer and select Manage.
  2. In the Server Manager Dashboard, click Add roles and features.
  3. Click Next and proceed to Server Roles.
  4. Ensure the following services and features are installed:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.