Windows Server 2019

  1. In the Start menu, right-click Computer and select Manage.
  2. In the Server Manager Dashboard, click Add roles and features.
  3. Click Next and proceed to Server Roles.
  4. Ensure the following services and features are installed:
    TIP: Click the image to open it in a separate tab for easier reading.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.