Windows 10

  1. In the Start menu, search for Turn Windows features on or off.
  2. Ensure the following features are installed:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.