Display Edit Log Report

Opens a report that displays all edits made to the currently open session or design.

Enabled

  • The open session or design must have an associated XML packet.

Execute

  1. Reads the XML packet.

  2. Converts XML packet contents for display in HTML window.

  3. Uses a style sheet to convert the XML packet edit log to HTML for display in a web browser.

    IMPORTANT: The style sheet location is determined by the following registry key: HKEY_LOCAL_MACHINE\Software\Miner and Miner\Process Framework\Style Sheets\EditHistoryXSLPath\

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.