Administrator Machine (Field Machines):

Create the following directory on the Administrator machine. When setup is complete, copy this directory structure (and the Process Framework databases) to all field machines. The paths on the Administrator machine and the field machines must be EXACTLY the same.

  • ProcessFramework: This is the directory where Engine Mobile sessions and designs are transported between the field and Enterprise. Make note of the path to this directory. In a later step, you'll create a configuration value (ProcessFrameworkField value) in the Process Framework database that points to this directory. If you do not create this directory and the configuration value, then Engine Mobile will automatically use this location instead: C:\Documents and Settings\<username>\Application Data\Miner and Miner\ProcessFrameworkField. All other folders shown in this directory are created automatically during the initial send/receive. This directory must be readable and writable. This directory may hold your field Process Framework Database, but it doesn't have to. You can place this database in another location.

Directories on the field machines require no special sharing or permissions.

QR code for this page

Was this helpful?