Server (Enterprise):

Create the following directory on the server or Enterprise machine. This directory does not have to be named exactly as shown. 

  • ProcessFramework: This directory must be created by an administrator on the Enterprise machine and be available for all client machines to access. It provides the necessary directory structure to transport Engine Mobile sessions and designs between the field and Enterprise. Make note of the path to this directory. In a later step, you'll create a configuration value (ProcessFrameworkEnterprise value) in the Process Framework database that points to this directory. All other folders shown in this directory are created automatically during the initial send/receive. No files in the ProcessFrameworkServer directory should ever be edited manually.

Once you have the directory structure set up on the server (Enterprise) machine, you will need to assign permissions to the ProcessFramework directory.

QR code for this page

Was this helpful?