DOCA0096EN-02

Circuit Breakers: Thermal Magnetic (TM-D) Protection

Introduction

Circuit breakers equipped with thermal-magnetic trip units are used for protection of cables on distribution systems supplied by transformers.

Thermal-magnetic trip units provide:

  • Thermal protection against overload with an adjustable pickup Ir, and a non-adjustable time-delay.

  • Magnetic protection against short circuits, with a fixed pickup Ii.

The following figure shows the tripping curve.

Ir Thermal protection pickup

Ii Instantaneous pickup

Thermal Protection (Ir)

The thermal protection pickup Ir is set by using a setting dial.

Turning the thermal protection adjustment dial (A) modifies the tripping curve (B), as shown.

The values of Ir are adjustable from 0.7 to 1 x In (circuit breaker rating) as shown in the following table:

Thermal protection

Circuit breaker rating In (A)

16

25

32

40

50

63

80

100

125

160

Pickup trip between 1.05 and 1.30 x Ir

Ir (A)

Adjustable in amps from 0.7 to 1 x In

Time delay (s)

tr (s)

Non-adjustable

Magnetic Protection (Ii)

The instantaneous pickup value Ii cannot be adjusted. Its value for each circuit breaker rating is shown in the following table:

Magnetic protection

Circuit breaker rating In (A)

16

25

32

40

50

63

80

100

125

160

Pickup ±20%

Ii (A)

500

600

600

600

600

800

1000

1250

1250

1250

The time delay for magnetic protection cannot be adjusted:

  • Non-tripping time: 10 ms

  • Maximum breaking time: 200 ms for I > 1.5 Ii

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.