Transfer a Parallel System from Normal Mode to Maintenance Bypass Mode
- From the home screen on the display select .
All UPSs will turn to static bypass mode.
- Turn the maintenance bypass breaker MBB to the ON (closed)
position.
The load is now supplied via the maintenance bypass breaker MBB.
- Turn the battery breakers BB of all UPSs to the OFF (open) position.
- Turn the unit input breakers UIB and the static switch input breakers SSIB of all UPSs to the OFF (open) position.
- Turn the unit output breakers UOB of all UPSs and the system isolation breaker SIB to OFF (open) position.
![]() |
---|
hazard of electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|