990-5940G-012

Caractéristiques des couples de serrage

Taille de vis Couple
M5 4 Nm
M6 5 Nm
M8 12 Nm
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Contenu utile ?