990-6409B-001

View the Logs

  1. On the display, select to select a log messages with the time mark.
  2. Use and to go through the list of logs.
    NOTE: C means an event is cleared or disappears, and S means an event is set or occurs.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.