990-6409B-001

Set the Battery Settings

NOTICE
risk of equipment damage
  • Only trained personnel following the required training course may undertake modifications to UPS system parameters.
  • The battery parameters must set according to the actual installation before starting up the UPS.
Failure to follow these instructions can result in equipment damage.
  1. On the display, select and then select Batt Settings.
  2. Enter the password 2334.
  3. Set the battery settings:
    1. Batt number: Verify the number of battery blocks is 20.
    2. Batt cap (AH): Set the battery capacity (battery block capacity (AH) x number of battery strings).
    3. Batt charge %: Set the battery charge percentage (between 1% and 15%).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.