990-6409B-001

Set the UPS Settings

NOTICE
risk of equipment damage
Only trained personnel following the required training course may undertake modifications to UPS system parameters.
Failure to follow these instructions can result in equipment damage.
  1. On the display, select and then select Setting.
  2. Enter the password 3526.
  3. Set the nominal input voltage (phase-neutral), the nominal output voltage (phase-neutral), and the nominal frequency.
    NOTE: Nom input PN and Nom output PN must have the same voltage rating.
  4. Restart the UPS to activate the settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.