990-6409B-001

Start up the UPS from Cold Start

NOTE
Cold start function is not a standard feature. If you want to have this feature, please contact SE for cold start kit (E3SOPT014) installation.
DANGER
hazard of electric shock, explosion, or arc flash
All electrical work must be performed by qualified personnel. Practice Lockout/Tagout procedures. Do not wear jewelry when working with electrical equipment.
Failure to follow these instructions will result in death or serious injury.
WARNING
HAZARD FROM MOVING PARTS
Keep hands, clothing, and jewelry away from moving parts. Check the equipment for foreign objects before closing the doors and starting the equipment.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
  1. After the cold start kit (E3SOPT014) is installed, wait for five minutes for the cold start capacitor to charge.
  2. Check and make sure that all the MBBs, UIBs ,SSIBs, and UOBs are in the OFF (open) position.
  3. Turn on the UOB.
  4. Press the cold start button for three seconds until the UPS starts up. The LED will light on the HMI.
  5. If the startup wizard pops up, follow the UPS operation manual to complete the setup. When the setup is completed, the UPS will output in normal mode automatically.
  6. If the startup wizard is disabled previously, the UPS will output in normal mode automatically.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.