990-6409B-001

Transfer a Single UPS from Maintenance Bypass Mode to Normal Mode

  1. Check that all breakers except the maintenance bypass breaker MBB are in the OFF (open) position.
  2. Reconnect the internal batteries of all UPSs and set all the battery breakers BB in the modular battery cabinets (if present) to the ON (closed) position.
  3. Turn the static switch input breaker SSIB to the ON (closed) position.

    The display turns on and the Home screen is shown.

  4. Turn the unit output breaker UOB to the ON (closed) position.

    The UPS starts up in static bypass mode.

  5. Turn the maintenance bypass breaker MBB to the OFF (open) position and reinstall the cover in front of the breaker.
  6. On the display select and then select Function > Clear alarm.
    NOTE: The system will not transfer to normal mode before the alarm has been cleared.
  7. Turn the unit input breaker UIB to the ON (closed) position.

    The rectifier ramps up. After UPS self-test, the battery relay closes automatically.

  8. When the rectifier LED turns steady green, the inverter synchronizes with bypass.
  9. Reinstall the cover on the maintenance bypass breaker MBB.
  10. After approximately 60 seconds, the UPS will automatically transfer to normal mode.

    The LEDs on the user interface show as follows:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.