990-6409B-001

Replace the Dust Filter

  1. Open the door.
  2. Loosen the screws and remove the metal brackets and the manual box.
  3. Replace the dust filter.
  4. Reinstall the metal brackets and fasten with the screws.
  5. Close the door.
  6. Reset the dust filter counter in the display. See Set the Life Cycle Monitoring for more information.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?