990-6409B-001

Start Up and Add a UPS to a Running Parallel System

Use this procedure to start up a UPS and add it to a running parallel system.

IMPORTANT: Before a UPS can be added to a parallel system, the parallel system must be configured by Schneider Electric.

  1. On the new UPS check that the UPS breakers (unit input breaker UIB, static switch input breaker SSIB, and unit output breaker UOB) are in the ON (closed) position.
  2. Reconnect the internal batteries of all UPSs and set all ModBC BBs (if present) to the ON (closed) position.
  3. Turn the external unit output breaker Ext. UOB of the UPS to the ON (closed) position.
  4. Turn the mains input breaker MIB and the bypass input breaker BIB of the UPS to the ON (closed) position.

    The display turns on and the Home screen is shown.

    When the UPS has initialized, the battery relay closes automatically. Close external battery breaker if external batteries are part of the system.

    The LEDs on the user interface show as follows:

  5. When the rectifier LED turns steady green, the UPS starts the inverter.

    The LEDs on the user interface show as follows:

  6. When the inverter LED turns steady green, the UPS automatically transfers to normal mode and joins the running parallel system.

    The LEDs on the user interface show as follows:

  7. Verify correct load sharing between the parallel UPS units.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.