990-6409B-001

Perform a Battery Test

The purpose of the battery test to verify the connection of the batteries and to check the battery capacity.

Prerequisite:

  • The bypass supply must be within specifications.

  • The battery capacity must be above 25%.

  • The battery voltage must be above 95% of the float voltage.

During the battery test, the system transfers to battery mode for approximately 30 seconds and then returns to normal mode.

  1. On the display, select and then select Battery test.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.