990-6409B-001

Register Your Easy UPS 3S

NOTE: The single Easy UPS 3S can also be registered using the mySchneider app which can be downloaded from App Store and Google Play.
  1. When prompted for registration, go to www.schneider-electric.com/contactsupport to find your local service contact number.
  2. On the display, select and then select Register*.
  3. Call Schneider Electric and provide your four-digit activation code.
  4. Type in the registration code provided by Schneider Electric.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.