Configure the Battery Solution
  TEHLİKE | 
               
|---|
| 
                      hazard of electrical shock, explosion, or arc flash 
                     Battery settings must only be configured by qualified
                        personnel knowledgeable of batteries, battery configuration, and the
                        required precautions. 
                     Bu talimatlara uyulmaması ölüm veya ciddi yaralanmaya neden olur. 
                   | 
               
- Tap .
 - Your battery solution type will be shown as:
- Standard if you have a standard battery solution from Schneider Electric the commercial reference for your specific battery configuration will be shown.
 - Custom if you have a custom battery solution.
 
 - Tap General settings and set up
                  the following parameters:NOT: On each page, tap OK to save your settings and tap the arrow symbol to go to the next page.
 - Only for custom battery solution: Tap Specific settings to view the following settings:NOT: These settings are only configurable by Schneider Electric Service.
Battery type Shows the configured battery type. Battery midpoint connected Shows if battery midpoint is connected. Disable temperature monitoring Shows if temperature monitoring is disabled. Allow boost charge Shows if boost charge is allowed. Boost şarj, boşalmış bir aküyü hızlı bir şekilde geri yüklemek için hızlı bir şarj işlemi yapmayı mümkün kılar.
Allow battery deep discharge Shows if battery deep discharge is allowed. The deep discharge function allows to discharge the batteries to an even lower voltage level than the normally recommended value when in battery operation. Note that this may damage the batteries. Enable battery automatic disconnect Shows if battery automatic disconnect is enabled. When the UPS output is off and no ability to charge the batteries is available, this function will trip the battery disconnect devices to avoid battery deep discharge after a period of: - 
                                       
Two weeks.
 - 
                                       
10 minutes with the battery cell voltage below the low battery shutdown level.
 
Capacity per battery block (Ah) Shows the battery capacity per battery block in ampere hours for the battery bank connected to each battery disconnect device. Number of parallel battery strings Shows the number of battery strings connected in parallel for the battery bank connected to each battery disconnect device. Number of battery blocks per string Shows the number of battery blocks per battery string. Number of battery cells per block Shows the number of battery cells per battery block. DC voltage per battery cell (V) Shows the float voltage. Float şarj, her tür aküde kullanılabilen ve şarj cihazı tarafından otomatik olarak başlatılan temel şarj işlevidir.
Shows the boost voltage. Boost şarj, boşalmış bir aküyü hızlı bir şekilde geri yüklemek için hızlı bir şarj işlemi yapmayı mümkün kılar.
Shows the equalization voltage. Eşitleme şarjı, eğri açık hücreli akülerin eşitlenmesinde kullanılır. Bu, mümkün olan en yüksek şarj voltajı seviyesi kullanılan şarj yöntemidir. Eşitleme şarjı yapılırken, şarj işlemi tamamlandığında değiştirilmesi gereken açık hücreli pillerden su buharlaşır.
Charge duration (sec) Shows the duration in seconds of the charge for Boost charging and Equalization charging. Nominal battery cell voltage (V) Shows the nominal voltage level per battery cell. DC shutdown voltage per battery cell (V) Shows the voltage level per battery cell for when the battery must be shut down. Nominal temperature Shows the nominal temperature in Celsius or Fahrenheit. Charge current rate Shows the charge current rate.  - 
                                       
 
 TEHLİKE