990-91263A-018

モジュール式バッテリーキャビネット1と内蔵バッテリー付き隣接UPSとの相互接続

  1. モジュール式バッテリーキャビネット1とUPSを所定の位置に押し込みます。
  2. モジュール式バッテリーキャビネット1とUPSの間に3つの相互接続ブラケットを取り付けます。
  3. モジュール式バッテリーキャビネット1とUPSの間に3つの相互接続ネジを取り付けます。
  4. モジュール式バッテリーキャビネット1とUPSの間に連結カバーを押し下げます。

    モジュール式バッテリーキャビネット1とUPS

フィードバック
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.