990-5810D-001

Connect the Signal Cables for Battery Solutions

Connect the Signal Cables between the I/O Cabinet and the Classic Battery Cabinets

NOTE: The illustration below shows a system with four battery banks each consisting of one classic battery cabinet. Connect signal cables according to the number of classic battery cabinets in your installation.
NOTE: If you have two classic battery cabinets in your battery bank, see Connect the Signal Cables between Two Classic Battery Cabinets in One Battery Bank for information on how to connect signal cables between two classic battery cabinets in one battery bank.
  1. Route the signal cables from the battery banks through the top or bottom of the I/O cabinet to the boards.
  2. Connect the signal cables between the I/O cabinet and the classic battery cabinets.

Connect the Signal Cables between Two Classic Battery Cabinets in One Battery Bank

NOTE: The procedure is identical for all battery banks with two classic battery cabinets.
  1. Remove the jumper between J3802 pin 3 and 4 in classic battery cabinet A.
  2. Connect the signal cables between classic battery cabinet A and classic battery cabinet B.

Connect Signal Cables between the I/O Cabinet and the Battery Breaker Cabinet

  1. Connect the below signal cables between the I/O cabinet and the battery breaker cabinet.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?