990-5810D-001

Install Busbars between the I/O Cabinet and the Power Cabinet

  1. Open the narrow door in the right side of the I/O cabinet.

    Front View of the I/O Cabinet

  2. Install the grounding busbar 880–5665 from the installation kit 0M–99046 between the I/O cabinet and the left-most power cabinet.
    NOTE: If the grounding busbar 880–5665 is not compatible with the power cabinet placed to the right of the I/O cabinet, the busbar kit 0J-0446 with flexible busbars must be used for the grounding connection instead of the grounding busbar. Contact Schneider Electric.

    Front View of the I/O Cabinet and the Power Cabinet

  3. Install the interconnection busbars from the installation kit 0H-9162 or 0H-9102 (supplied with the power cabinet) between the I/O cabinet and the left-most power cabinet.

    Front View of the I/O Cabinet and the Power Cabinet

    1. Install the battery- interconnection busbar 0M-819336.

      Front View of Busbar Connections

    2. Install the three input interconnection busbars 0M-97885.
    3. Install the battery+ interconnection busbar 0M-140035.

      Front View of Busbar Connections

    4. Install the three output interconnection busbars 0M-97886.
    5. Install the neutral interconnection busbar 880–10146 or 880–9720.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?