990-5810D-001

Mount the Front Anchoring Bracket

  1. Fasten the front anchoring brackets to the front of the cabinets using the provided bolts.

    Front View of the I/O Cabinet and Two Power Cabinets

  2. Anchor the front anchoring brackets to the floor.
    NOTE: Floor anchoring bolts are not supplied.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?