Position the Cabinets
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
Do not step/walk on top of the cabinets.
Failure to follow these instructions will result in death or serious injury.
|
- Install the interconnection cover from the installation kit 0M-99582 on the right side (front view) of the right-most power cabinet and fasten with the M6 nuts.
- Move the side panel from the right side (front view) of the I/O cabinet and install it on the right side of the right-most power cabinet.
- Perform the following steps on all power cabinets:
- Remove the 12 screws and open the fan door of the power cabinets.
- Disconnect the cable between the fan door and the power cabinet.
- Lift the fan door up and remove it.
- Disconnect the two cables from each of the two middle power blocks.
- Loosen the screws and pull out the middle power blocks.
Be careful not to damage the cables.
NOTICE risk of equipment damageCover the power blocks when removed from the power cabinet to avoid dust in the power blocks.Failure to follow these instructions can result in equipment damage. - Loosen the screws and remove the plate below the power blocks.
- Install the fan doors temporarily on all power cabinets and fasten with two screws.
- Push the I/O cabinet and the power cabinets one by one into position against the rear anchoring brackets – the cabinets will connect to the conic outcroppings on the brackets.
- Fasten the cabinets to the rear anchoring brackets by tightening the bolts on the front of the cabinet. Torque to 50 Nm (36.87 lb-ft).
- Remove the fan doors of the power cabinets.
- Lower the two front feet on all cabinets until they connect with the floor – use a bubble-leveler to ensure that the cabinets are level. Use the provided levelling shims if necessary.
- Install the top baying bracket on the top of the cabinets and fasten with the provided screws.
- Mount the M6 screws from the installation kit from right to left in the five marked positions between the power cabinets and in the four marked positions between the power cabinet and the I/O cabinet to tighten the cabinets together.
DANGER