Remove the I/O Cabinet from the Pallet
| NOTICE |
|---|
|
RISK of equipment damage
Ensure that the floor is level and can support the weight
of the jack when it carries the cabinet.
Failure to follow these instructions can result in equipment damage.
|
| NOTICE |
|---|
|
RISK of equipment damage
Be careful not to damage the cabinets when using the jack.
Failure to follow these instructions can result in equipment damage.
|
- Take the installation kit 0M-816661 shipped with the I/O cabinet.
- Lift up and remove the front anchoring bracket. Save it for later use.
- Loosen the bolts and remove the rear anchoring bracket. Save it for later use.
- Place the floor protection plate under the pallet on the rear of the cabinet.
- Place the jack from the installation kit in the hole in
the transport bracket on the rear of the cabinet.
WARNINGhazard of TiltingDo not use a jack in the front and rear transport bracket at the same time.Failure to follow these instructions can result in death, serious injury, or equipment damage. - Loosen the screws and remove the two indicated brackets.
- Loosen the screws from the rear transport bracket and from the middle pallet part. Save the two middle pallet parts for step 11.
- Use a drilling machine with the provided hexagonal socket
to activate the jack, slide it into position in the bracket, and to
make contact with the floor protection plate.NOTE: Reduce the drill torque to minimum to prevent kickback.
- Use the jack to lift the pallet to the top position.
- Remove the rear and middle pallet parts.
- Place the two middle pallet parts removed in step 7 under the transportation bracket.
- Use a drilling machine to lower the cabinet down onto the support.
- Move the floor protection plate and the jack from the rear to the front side.
- Loosen and remove the bolts from the front transport bracket.
- Use a drilling machine with the provided hexagonal socket to activate the jack, slide it into position in the bracket, and to lift the pallet to the top position.
- Remove the front pallet parts.
- Use the jack to lower the cabinet onto the floor until the wheels connect with the floor. Remove the jack and the floor protection plate.
- Wheel the cabinet away and remove the remaining pallet parts.
- Remove the indicated brackets from both the front and the
rear side of the I/O cabinet.
The cabinet can now be moved on the built-in wheels to the installation area.