990-5810D-001

Prepare the I/O Cabinet for Power Cables in Top Cable Entry Systems

  1. Open the front doors of the I/O cabinet.
  2. Loosen the screws and open the inner door.

    Front View of the I/O Cabinet

  3. Remove the metal plate.

    Front View of the I/O Cabinet

  4. Remove the plastic plate.
  5. Loosen the bolts and remove the gland plate from the top of the I/O cabinet

    Front View of the I/O Cabinet

  6. Drill or cut holes for cables/conduits in the top gland plate according to the guidelines.
    DANGER
    hazard of electric shock, explosion, or arc flash
    Do not drill/punch holes for cables or conduits with the gland plates installed and do not drill/punch holes in close proximity to the UPS.
    Failure to follow these instructions will result in death or serious injury.
  7. Install conduits and reinstall the top gland plate.
    DANGER
    hazard of electric shock, explosion, or arc flash
    Ensure that there are no sharp edges that can damage the cables.
    Failure to follow these instructions will result in death or serious injury.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?