Mount the Rear Anchoring Brackets
DANGER |
|---|
|
hazard of tilting
All rear and front anchoring brackets must be installed.
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
Leave the UPS system covered while making anchoring holes
to prevent dust or other conductive particles from entering the system.
Failure to follow these instructions will result in death or serious injury.
|
- Place the rear anchoring brackets of the I/O cabinet and the power cabinets in the final installation area.
- Interconnect the rear anchoring brackets using the provided screws and bolts.
- Mark the hole locations.
- Drill anchoring holes according to national and local requirements.
- Mount the rear anchoring brackets to the floor. Bolts are not supplied.
- Use a bubble-leveler to ensure that the brackets are level. Use the provided leveling shims if necessary.
DANGER