990-5810D-001

Install the Single Utility/Mains Kit

NOTE: This procedure is only applicable to single utility/mains systems.
  1. Install the single utility/mains kit between the input and bypass busbars. Connect L1 to L1, L2 to L2, and L3 to L3.
    NOTE: Two 880–9642 busbars are required for each connection.

    Top Front View of the Power Connection Area in the I/O Cabinet

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?