990-5810D-001

Connect the Signal Cables between the I/O Cabinet and the Power Cabinets

  1. Open the narrow door.

    Front View of the I/O Cabinet and the Left-Most Power Cabinet

  2. Remove the indicated plate from the I/O cabinet.
  3. Remove the three indicated plates from the power cabinets.
  4. Route and connect the two system power supply cables 0W11379 shipped in the power cabinets.

    Front View of the I/O Cabinet and the Left-Most Power Cabinet

    1. Connect the signal cable 0W11379 from X0002 in the left-most power cabinet to X0001 in the I/O cabinet.
    2. Connect the signal cable 0W11379 from X0002 in the second power cabinet to X0001 in the left-most power cabinet.
  5. Open the wide door in the I/O cabinet.
  6. Remove the plate in front of the cable channel.

    Front View of the I/O Cabinet

  7. Remove the plate in front of the communication board.
  8. Connect the signal cables in the power cabinets:
    NOTE: Minimum bending radius is 50 mm.

    Front View of the I/O Cabinet and Two Power Cabinets

    1. Connect 0W11378 to 640–6515 J1005 in power cabinet 1.
    2. Connect 0W11384 to 640–6515 J1005 in power cabinet 2.
    3. Connect 0W11385 to 640–6515 J1005 in power cabinet 3 if available.
    4. Connect 0W12213 to 640–6515 J1005 in power cabinet 4 if available.
    5. Connect 0W98928 to 640–6515 J1005 in power cabinet 5 if available.
  9. Route the signal cables into the I/O cabinet as shown.
  10. Remove and dispose of the plastic plate below the terminals.

    Front View of the I/O Cabinet

  11. Route the signal cables as shown on the illustration and fasten with the provided cable ties.
  12. Open the door to ensure that the cables will not be too tight and connect the signal cables in the I/O cabinet and fasten with the provided cable ties:
    NOTE: Minimum bending radius is 50 mm.
    1. Connect 0W11378 to 640–6502 J1100.
    2. Connect 0W11384 to 640–6502 J1101.
    3. Connect 0W11385 to 640–6502 J1102.
    4. Connect 0W12213 to 640–6502 J1103.
    5. Connect 0W98928 to 640–6502 J1104.
  13. Reinstall the plate in front of the communication board.

    Front View of the I/O Cabinet

  14. Reinstall the plate in front of the cable channel.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?