990-6264H-001

PBUS Cable Connections (Board 0P3643)

NOTE: The PBUS 1 cables are white and the PBUS 2 cables are red.
NOTE: The total length of the PBUS cables must not exceed 60 m (197 ft).

Example of System with Four UPSs in Parallel

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.