990-6264H-001

Position the Cabinets

DANGER
hazard of electric shock, explosion, or arc flash
Do not step/walk on top of the cabinets.
Failure to follow these instructions will result in death or serious injury.
  1. Install the cover from installation kit 0M-98993 on the right-most power cabinet.
  2. Move the side panel from the right side of the I/O cabinet and install it on the right-most power cabinet.
    WARNING
    Hazard of arc flash
    • Do not make mechanical changes to the product (including removal of cabinet parts or drilling/cutting of holes) that are not described in the installation manual.
    • Move and install the indicated side panel in all installation types (including parallel installations with no air gap between the frames or in installations where the right-most power cabinet is placed against a wall).
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
  3. Open the two inner doors of the I/O cabinet.
  4. Remove the two rear bottom plates.
  5. Push the I/O cabinet into position against the rear anchoring bracket - the I/O cabinet will connect to the conic outcroppings on the rear anchoring bracket.
  6. Fasten the cabinet to the rear anchoring bracket by tightening the bolts. Torque to 50 Nm (36.87 lb-ft).
  7. Reinstall the two rear bottom plates.
  8. Push the power cabinets one by one into position against the rear anchoring brackets – the cabinets will connect to the conic outcroppings on the brackets.
    CAUTION
    risk of equipment damage
    When pushing the power cabinet into position, push on the frame to avoid damaging the signal cables.
    Failure to follow these instructions can result in injury or equipment damage.
  9. Fasten the power cabinets to the rear anchoring brackets by tightening the bolts on the front of the power cabinet. Torque to 50 Nm (36.87 lb-ft).
  10. Lower the two front feet on all cabinets until they connect with the floor – use a bubble-leveler to ensure that the cabinets are level. Use the provided levelling shims if necessary.
  11. Install the top baying bracket on the top of the cabinets and fasten with the provided screws.

    I/O Cabinet and Two Power Cabinets

  12. Mount the M6 screws from the installation kit from right to left in the five marked positions between the power cabinets and in the four marked positions between the power cabinet and the I/O cabinet to interconnect the cabinets.

    From Power to Power Cabinet

    From Power to I/O Cabinet

  13. Verify that the right-most power cabinet for the I/O cabinet has the cover 0M-98993 and the side panel installed before continuing.

    1250 kW I/O with Maximum Number of Power Cabinets

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.