990-6264H-001

Remove the Front Doors for Easier Access (Optional)

NOTE: During installation and maintenance, doors may be removed to meet the working space requirements per local and national electric codes.
  1. Open the door.
  2. Lift the door upwards until it clears the hinge pins and remove the door.

    Front View of the I/O Cabinet

    Front View of the Power Cabinet

  3. Store the door securely until reinstallation.
    NOTE: The hinge pin is loose and may come off with the door – reinsert it in the door hinge for reinstallation of the door.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?