990-6264H-001

Connect Cables to the External Supply for Lithium-ion Battery Solution (Optional)

Depending on your chosen configuration, the 1250 kW I/O cabinet may not have the battery control disconnect devices preinstalled. If needed, the Galaxy VX Lithium-ion BMS Power Supply Kit (GVXOPT002) can be ordered and installed on site.

DANGER
hazard of electric shock, explosion, or arc flash
Do not drill/punch holes for cables or conduits with the gland plates installed and do not drill/punch holes in close proximity to the UPS.
Failure to follow these instructions will result in death or serious injury.

The rating of the external supply disconnect device is 6.3 A.

Cable Sizes for External Supply

  Conductors per Phase PE Conductor/Equipment Grounding Conductor Conduit
Cable sizes for 400 V systems 1.5 mm² 1.5 mm² NA
Cable sizes for 480 V systems* 1x12-18 AWG 1x18 AWG 0.5 in
  1. Follow the procedure Prepare the I/O Cabinet for Power Cables in Top Cable Entry Systems to prepare the top gland plate for cables.
  2. Open the indicated door and remove the covers in front of the battery control disconnect devices.
  3. Connect the cables from the equipment to be supplied by the UPS.
  4. Reinstall the covers in front of the battery control disconnect devices.
  5. Close the door.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.