990-6264H-001

Installation Kits Shipped with the Power Cabinet

Installation Kit 0H-9102

NOTE: These installation kit parts are shipped in the packaging of the power cabinet.
Part Used in Number of Units
Rear anchoring bracket for power cabinet 0M-818242 Mount the Rear Anchoring Brackets

1

M8 x 20 hexagonal torx with washer
803–8590

2

Front anchoring bracket for power cabinet 0M-816684 Mount the Front Anchoring Brackets

1

Long top baying bracket 0M-821220 Position the Cabinets

1

M6 x 16 torx screw with washer
803–0686

15

M10 nut with washer
803–1005

24

M10 x 35 hexagonal torx with washer
803–8587

12

1 mm leveling shims
870-98678

10

Ground interconnection busbar 880-99027 Save for the field service representative. The busbars will be installed by Schneider Electric during assembly service.

1

M8 nut with washer
803-8007

4

M8 x 35 mm hexagonal torx with washer
803-8588

4

Interconnection busbar 880-10146 and 880-9720 from power cabinet to power cabinet (neutral)

1

Interconnection busbar 0M-140035 power cabinet to power cabinet (battery +)

1

Interconnection busbar 0M-97886 power cabinet to power cabinet (output)

3

Interconnection busbar 0M-819336 power cabinet to power cabinet (battery -)

1

Interconnection busbar 0M-97885 power cabinet to power cabinet (input)

3

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.