990-6264F-001

Galaxy VXUPS with 1250 kW I/O CabinetInstallation

380 V, 400 V, 415 V, 440 V, and 480 V

500 kW/kVA, 500 kW/kVA N+1, 625 kW/kVA, 800 kW/kVA
500 kW/kVA Expandable to 750 kW/kVA, 750 kW/kVA, 750 kW/kVA N+1
500 kW/kVA, 625 kW/kVA, 750 kW/kVA Expandable to 1000 kW/KVA, 1000 kW/kVA, 1000 kW/kVA N+1
1100 kW/kVA, 1100 kW/kVA N+1
500 kW/kVA, 750 kW/kVA, and 1000 kW/kVA Expandable to 1250 kW/kVA, 1250 kW/kVA, 1250 kW/kVA, 1250 kW/kVA N+1

11/2024

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?