990-6264H-001

Installation Kits Shipped with the I/O Cabinet

Installation Kit 0M-816661

Part

Used in

Number of units

Jack

0M-815326

Follow the receiving and unpacking manual to remove the cabinets from the pallet using this installation kit.

1

Floor protection plate

870-25867

1

Hexagonal socket for drilling machine

815–7044

1

Installation Kit 0H-9385

Part Used in Number of Units
Angle for right side of the rear anchoring bracket 870-30412 Mount the Rear Anchoring Brackets

1

M8 x 20 hexagonal torx with washer
803-8590

2

1 mm leveling shims
870-96678

30

EMC cover right 0M-98993 Position the Cabinets

1

M6 nut with washer
803–5022

8

M10 x 45 hexagonal torx with washer
803-9727
Save for the field service representative. They will be used for fastening the busbars and will be installed by Schneider Electric during assembly service.

16

M8 x 35 hexagonal torx with washer
803-8588

2

M10 x 35 bolt with washer
803-9795

4

Terminator for modbus
750-0532
Modbus Connections (Board 0P6502)

2

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.