990-6264H-001

Recommended Upstream Protection and Cable Sizes – IEC

DANGER
hazard of electric shock, explosion, or arc flash
An easily accessible disconnect device is required for upstream protection. Maximum fault current disconnection time: 46 seconds at 200% input.
Failure to follow these instructions will result in death or serious injury.
NOTE: Overcurrent protection is to be provided by others.

Cable sizes in this manual are based on table B.52.12 and B.52.13 of IEC 60364-5-52 with the following assertions:

  • 90 °C conductors

  • An ambient temperature of 30 °C

  • Use of copper or aluminum conductors

  • Installation method F4 for DC cables and installation method F5 for AC cables, corrected for single layer in perforated cable tray.

PE cables are sized in accordance with IEC 60364-5-54 table 54.2 Minimum cross-sectional area of protective conductors.

NOTE: Always consider the PE size according to the complete electrical installation. Minimum size of the PE conductor must comply with local safety regulations for high PE conductor current equipment.

If the ambient temperature is greater than 30 °C, larger conductors are to be selected in accordance with the correction factors of the IEC.

NOTE: The use of aluminum conductors can limit the number of parallel Lithium-ion battery cabinets. Contact Schneider Electric for more information.
NOTICE
Risk of equipment damage
To ensure correct load sharing in bypass operation in a parallel system, the following recommendations apply:
  • The bypass cables must be of the same length for all UPSs.
  • The output cables must be of the same length for all UPSs.
  • The input cables must be of the same length for all UPSs in a single mains system.
  • Cable formation recommendations must be followed.
  • The reactance of busbar layout in the bypass/input and output switchgear must be the same for all UPSs.
If the above recommendations are not followed the result can be uneven load sharing in bypass and overload of individual UPSs.
Failure to follow these instructions can result in equipment damage.
NOTICE
Risk of unintentional device operation
If a residual current-operated protective device (RCD-B) is used upstream as ground fault protection, then the RCD-B shall be sized to not trip on the leakage current of this product. The start-up leakage current can be up to 3 A. The continuous maximum leakage current is 350 mA.
Failure to follow these instructions can result in equipment damage.

Upstream Protection for IEC and Minimum Prospective Phase-To-Earth Short Circuit at the UPS Input/Bypass Terminals

DANGER
Hazard of electric shock, explosion, or arc flash
The upstream overcurrent protective device (and its settings) must be sized to ensure a disconnecting time within 0.2 seconds for a minimum prospective phase-to-earth short circuit current calculated or measured at the input/bypass terminals of the UPS.
Failure to follow these instructions will result in death or serious injury.
If the upstream overcurrent protective device is a circuit breaker with adjustable short time protection, then it is possible to adjust the short time protection current and short time delay (if present) to meet the requirement of 0.2 seconds for a calculated or measured phase-to-earth prospective short circuit current at the input/bypass terminals of the UPS.

Recommended Upstream Protection and Cable Sizes for 500 kW UPS

  Maximum OCPD (A) Cable size per phase (mm2)
Copper / Aluminum
PE cable size (mm2)
Copper / Aluminum
Voltage (V) 380 400 415 440 380 400 415 440 380 400 415 440
Input 1000
Ir=0.90
1000
Ir=0.90
1000
Ir=0.90
1000
Ir=0.90
2x240/
3x185
2x240/
3x185
2x240/
3x185
2x240/
3x185
1x240/
2x150
1x240/
2x150
1x240/
2x150
1x240/
2x150
Bypass 800
Ir=0.98
800
Ir=0.95
800
Ir=0.9
800
Ir=0.9
2x185/
2x240
2x150/
2x240
2x150/
2x240
2x150/
2x240
1x185/
1x240
1x150/
1x240
1x150/
1x240
1x150/
1x240
Output 800
Ir=0.98
800
Ir=0.95
800
Ir=0.9
800
Ir=0.9
2x185/
2x240
2x150/
2x240
2x150/
2x240
2x150/
2x240
1x185/
1x240
1x150/
1x240
1x150/
1x240
1x150/
1x240
Battery 1500 1500 1500 1500 3x185/
3x240
3x185/
3x240
3x185/
3x240
3x185/
3x240
2x150/
2x185
2x150/
2x185
2x150/
2x185
2x150/
2x185

Recommended Upstream Protection and Cable Sizes for 625 kW UPS

  Maximum OCPD (A) Cable size per phase (mm2)
Copper / Aluminum
PE cable size (mm2)
Copper / Aluminum
Voltage (V) 380 400 415 440 380 400 415 440 380 400 415 440
Input

1250
Ir=0.9

1250
Ir=0.9

1250
Ir=0.9

1250
Ir=0.9
3x185/
3x240
3x185/
3x240
3x185/
3x240
3x185/
3x240
2x150/
2x185
2x150/
2x185
2x150/
2x185
2x150/
2x185
Bypass 1000
Ir=0.98
1000
Ir=0.95
1000
Ir=0.9
1000
Ir=0.9
2x240/
3x240
2x240/
3x185
2x240/
3x185
2x240/
3x185
1x240/
2x185
1x240/
2x150
1x240/
2x150
1x240/
2x150
Output 1000
Ir=0.98
1000
Ir=0.95
1000
Ir=0.9
1000
Ir=0.9
2x240/
3x240
2x240/
3x185
2x240/
3x185
2x240/
3x185
1x240/
2x185
1x240/
2x150
1x240/
2x150
1x240/
2x150
Battery 2000 2000 2000 2000 3x240/
4x240
3x240/
4x240
3x240/
4x240
3x240/
4x240
2x185/
2x240
2x185/
2x240
2x185/
2x240
2x185/
2x240

Recommended Upstream Protection and Cable Sizes for 750 kW UPS

  Maximum OCPD (A) Cable size per phase (mm2)
Copper / Aluminum
PE cable size (mm2)
Copper / Aluminum
Voltage (V) 380 400 415 440 380 400 415 440 380 400 415 440
Input 1600
Ir=0.9
1600
Ir=0.9
1600
Ir=0.9
1250
Ir=1.0
3x240/
4x240
3x240/
4x240
3x240/
4x240
3x185
4x240
2x185/
2x240
2x185/
2x240
2x185/
2x240
2x150/
2x240
Bypass 1250
Ir=0.95
1250
Ir=0.9
1250
Ir=0.9
1000
Ir= 1.0
3x185/
4x185
3x185/
3x240
3x185/
3x240
2x240/
3x240
2x150/
2x185
2x150/
2x185
2x150/
2x185
1x240/
2x185
Output 1250
Ir=0.95
1250
Ir=0.9
1250
Ir=0.9
1000
Ir=1.0
3x185/
4x185
3x185/
3x240
3x185/
3x240
2x240/
3x240
2x150/
2x185
2x150/
2x185
2x150/
2x185
1x240/
2x185
Battery 2500 2500 2500 2500 4x240/
5x240
4x240/
5x240
4x240/
5x240
4x240/
5x240
2x240/
3x240
2x240/
3x240
2x240/
3x240
2x240/
3x240

Recommended Upstream Protection and Cable Sizes for 800 kW UPS

  Maximum OCPD (A) Cable size per phase (mm2)
Copper / Aluminum
PE cable size (mm2)
Copper / Aluminum
Voltage (V) 380 400 415 440 380 400 415 440 380 400 415 440
Input 1600
Ir=0.9
1600
Ir=0.9
1600
Ir=0.9
1600
Ir=0.9
3x240/
4x240
3x240/
4x240
3x240/
4x240
3x240/
4x240
2x185/
2x240
2x185/
2x240
2x185/
2x240
2x185/
2x240
Bypass 1250
Ir=1.0
1250
Ir=0.95
1250
Ir=0.9
1250
Ir=0.9
3x185/
4x240
3x185/
4x185
3x185/
3x240
3x185/
3x240
2x150/
2x185
2x150/
2x185
2x150/
2x185
2x150/
2x185
Output 1250
Ir=1.0
1250
Ir=0.95
1250
Ir=0.9
1250
Ir=0.9
3x185/
4x240
3x185/
4x185
3x185/
3x240
3x185/
3x240
2x150/
2x185
2x150/
2x185
2x150/
2x185
2x150/
2x185
Battery 2500 2500 2500 2500 4x240/
5x240
4x240/
5x240
4x240/
5x240
4x240/
5x240
2x240/
3x240
2x240/
3x240
2x240/
3x240
2x240/
3x240

Recommended Upstream Protection and Cable Sizes for 1000 kW UPS

  Maximum OCPD (A) Cable size per phase (mm2)
Copper / Aluminum
PE cable size (mm2)
Copper / Aluminum
Voltage (V) 380 400 415 440 380 400 415 440 380 400 415 440
Input 2000
Ir=0.9
2000
Ir=0.9
2000
Ir=0.9
2000
Ir=0.9
4x240/6x240 4x240/6x240 4x240/6x240 4x240/6x240 2x240/3x240 2x240/3x240 2x240/3x240 2x240/3x240
Bypass 1600
Ir=0.98
1600
Ir=0.95
1600
Ir=0.9
1600
Ir=0.9
4x185/5x240 4x185/5x240 3x240/4x240 3x240/4x240 2x185/3x240 2x185/3x240 2x185/2x240 2x185/2x240
Output 1600
Ir=0.98
1600
Ir=0.98
1600
Ir=0.9
1600
Ir=0.9
4x240/6x240 4x240/6x240 3x240/6x240 3x240/6x240 2x240/3x240 2x240/3x240 2x240/3x240 2x240/3x240
Battery 3300 3300 3300 3300 5x240/7x240 5x240/7x240 5x240/7x240 5x240/7x240 3x240/4x240 3x240/4x240 3x240/4x240 3x240/4x240

Recommended Upstream Protection and Cable Sizes for 1100 kW UPS

NOTE: For a 1250 I/O cabinet, it is preferred to use flexible copper power cables with as small a diameter as possible. The number of power cables needed for this kW rating will make large and inflexible power cables more difficult to install.
  Maximum OCPD (A) Cable size per phase (mm2)
Copper / Aluminum
PE cable size (mm2)
Copper / Aluminum
Voltage (V) 380 400 415 440 380 400 415 440 380 400 415 440
Input 2000
Ir=0.98
2000
Ir=0.98
2000
Ir=0.98
2000
Ir=0.95
4x300/
5x300
4x300/
5x300
4x300/
5x300
4x300/
5x300
2x300/
3x300
2x300/
3x300
2x300/
3x300
2x300/
3x300
Bypass 2000
Ir=0.9
2000
Ir=0.9
1600
Ir=0.98
1600
Ir=0.95
4x240/
5x300
4x240/
5x300
3x300/
4x300
3x300/
4x300
2x240/
3x300
2x240/
3x300
2x240
2x300
2x240/
2x300
Output 2000
Ir=0.9
2000
Ir=0.9
1600
Ir=0.98
1600
Ir=0.95
4x240/
5x300
4x240/
5x300
3x300/
4x300
3x300/
4x300
2x240/
3x300
2x240/
3x300
2x240
2x300
2x240/
2x300
Battery 3300 3300 3300 3300 5x300/
7x300
5x300/
7x300
5x300/
7x300
5x300/
7x300
3x300/
4x300
3x300/
4x300
3x300/
4x300
3x300/
4x300

Recommended Upstream Protection and Cable Sizes for 1250 kW UPS

NOTE: For a 1250 I/O cabinet, it is preferred to use flexible copper power cables with as small a diameter as possible. The number of power cables needed for this kW rating will make large and inflexible power cables more difficult to install.
  Maximum OCPD (A) Cable size per phase (mm2)
Copper / Aluminum
PE cable size (mm2)
Copper / Aluminum
Voltage (V) 380 400 415 440 380 400 415 440 380 400 415 440
Input 2500
Ir=0.9
2500
Ir=0.9
2500
Ir=0.9
2500
Ir=0.9
5x240/
6x300
5x240/
6x300
5x240/
6x300
5x240/
6x300
3x240/
3x300
3x240/
3x300
3x240/
3x300
3x240/
3x300
Bypass 2000
Ir=0.98
2000
Ir=0.95
2000
Ir=0.9
2000
Ir=0.9
4x300/
5x300
4x300/
5x300
4x240/
5x300
4x240/
5x300
2x300/
3x300
2x300/
3x300
2x240/
3x300
2x240/
3x300
Output 2000
Ir=0.98
2000
Ir=0.95
2000
Ir=0.9
2000
Ir=0.9
4x300/
5x300
4x300/
5x300
4x240/
5x300
4x240/
5x300
2x300/
3x300
2x300/
3x300
2x240/
3x300
2x240/
3x300
Battery 4000 4000 4000 4000 6x300/
7x300
6x300/
7x300
6x300/
7x300
6x300/
7x300
3x300/
4x300
3x300/
4x300
3x300/
4x300
3x300/
4x300

Recommended Bolt and Lug Sizes for IEC

Cable size mm2 Bolt size Cable lug type
16 M10 x 40 mm TLK 16-10
25 M10 x 40 mm TLK 25-10
35 M10 x 40 mm TLK 35-10
50 M10 x 40 mm TLK 50-10
70 M10 x 40 mm TLK 70-10
95 M10 x 40 mm TLK 95-10
120 M10 x 40 mm TLK 120-10
150 M10 x 40 mm TLK 150-10
185 M10 x 40 mm TLK 185-10
240 M10 x 40 mm TLK 240-10
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?