990-6264H-001

Route the Signal Cables between the I/O Cabinet and the Power Cabinets

NOTE: Do not connect the signal cables. Signal cables will be connected by Schneider Electric during the assembly service.

Overview of Signal Cables between the I/O Cabinet and the Power Cabinets

  1. Remove the indicated plates from the I/O cabinet and all the power cabinets.
  2. Route signal cable 0W11379 from X0002 in the power cabinet 2 to X0001 in power cabinet 1.
  3. Route the signal cable 0W13003 preconnected in the right side of the I/O cabinet to X0002 in power cabinet 1.
  4. Open the left inner door and remove the indicated plate from the door.
  5. Route the signal cables 0W13022 (power cabinets 1-3) and 0W13010 (power cabinets 4-6) from the J1005 terminals in the power cabinets to the I/O cabinet.
    NOTE: Minimum bending radius is 50 mm.
  6. Route the signal cables 0W13022 and 0W13010 to the board 0P6502 in the left door.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.