990-6264H-001

Signal Cable Connections to the Switchgear (Boards 0P6547, 0P6548, 0P6549)

NOTE: The unit output disconnect device UOB must include two separated AUX switches.
NOTE: The solenoid key release unit (SKRU) is only applicable to 480 V systems.

All circuits connected must have the same 0 V reference.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.