990-6264H-001

Overview of Input Contacts and Output Relays

Input Contacts

Do not connect any circuit to the input contacts unless it can be confirmed that the circuit is Class 2/SELV.

All circuits connected must have the same 0 V reference.

The input contacts support 24 VDC 10 mA.

The switch SW5500 on 0P6548 is used to select between internal SELV supply for inputs (standard setting) and external supply*. If external supply is selected, the supply must be connected to J5530.

Name Description Location
IN 1 (Contact 1) Configurable input contact 0P6548 terminal J5502*
IN 2 (Contact 2) Configurable input contact 0P6548 terminal J5503*
IN 3 (Contact 3) Configurable input contact 0P6548 terminal J5504*
IN 4 (Contact 4) Configurable input contact 0P6548 terminal J5505*
IN 5 (Contact 5) Configurable input contact 0P6548 terminal J5510*
IN 6 UOB redundant AUX contact 0P6548 terminal J5509*
IN 7 Transformer temperature switch 0P6548 terminal J5508*
IN 8 External bonding contact 0P6548 terminal J5507*
IN 9 Forced external synchronization input 0P6548 terminal J5506*
IN 10 External synchronization requested 0P6548 terminal J5511*
IN 11 Use static bypass standby 0P6548 terminal J5512*
IN 14 MegaTie 0P6552 terminal J9027*

Output Relays

NOTE: Maximum 250 VAC 5 A must be connected to the output relays.

All external circuitry must be fused with maximum 5 A fast acting fuses.

Name Description Location
OUT 1 (Relay 1) Configurable output relay 0P6547 terminal J4939
OUT 2 (Relay 2) Configurable output relay 0P6547 terminal J4940
OUT 3 (Relay 3) Configurable output relay 0P6547 terminal J4941
OUT 4 Forced external synchronization output 0P6548 terminal J5520*
OUT 5 MegaTie 0P6548 terminal J5521*
OUT 6 External synchronization requested output 0P6548 terminal J5522*
OUT 7 UPS in inverter ON 0P6548 terminal J5523*
OUT 8 (Relay 4) Configurable output relay 0P6548 terminal J5524*
OUT 9 (Relay 5) Configurable output relay 0P6548 terminal J5525*
OUT 10 (Relay 6) Configurable output relay 0P6548 terminal J5528*
OUT 14 Bonding contactor 0P6552 terminal J9029*
NOTE: Refer to the operation manual for configuration options.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.