990-914301A-001

Clearance

NOTE: Clearance dimensions are published for airflow and service access only. Consult with the local safety codes and standards for additional requirements in your local area.
NOTE: The UPS (I/O cabinet and power cabinets) can be placed up against a wall and there is no requirement for rear or side access.
NOTE: Clearance dimensions of Lithium-ion Battery Cabinet have been verified by UL 9540A 4th edition (project No. 4789548397, issued by UL on 2021-05-21).

UPS with 1250 kW I/O Cabinet

Lithium-ion Battery Cabinet

* Rear clearance is only required for Lithium-ion battery cabinet with seismic anchoring.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?