990-914301A-001

Mount the Front Anchoring Brackets

  1. Fasten the front anchoring brackets to the front of the cabinets using the provided bolts.
  2. Anchor the front anchoring brackets to the floor.
    NOTE: Floor anchoring bolts are not supplied.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?