Recommended Upstream Protection and Cable Sizes
CAUTION |
|---|
|
hazard of fire
Failure to follow these instructions can result in injury or equipment damage.
|
Cable sizes in this manual are based on Table 310.15 of the National Electrical Code 2014 (NEC) with the following assertions:
-
90 °C (194 °F) conductors (THHN) for 75 °C (167 °F) termination
-
Not more than 3 current carrying conductors in each conduit
-
An ambient temperature of max. 30 °C (86 °F)
-
Use of copper or aluminum conductors for the UPS.
-
Use of copper conductors for the Lithium-ion cabinet.
-
100% rated breakers
-
Nominal operating conditions
If the ambient room temperature is greater than 30 °C (86 °F), use larger or additional parallel conductors in accordance with the correction factors of the NEC. The maximum allowable conductor size is 600 kcmil.
Equipment Grounding Conductors (EGC) are sized in accordance with NEC Article 250.122 and Table 250.122 Minimum size equipment conductor for grounding equipment.
| NOTICE |
|---|
|
Risk of equipment damage
To ensure correct load sharing in bypass operation in
a parallel system, the following recommendations apply:
Failure to follow these instructions can result in equipment damage.
|
Recommended Upstream Protection and Cable Sizes for 500 kW UPS
| Maximum OCPD (A) | Cable size per phase (AWG/kcmil) Copper / Aluminum |
EGC cable size (AWG/kcmil)* Copper / Aluminum |
|
|---|---|---|---|
| Input | 800 (Ir = 1.0) | 2x500 / 3x400 | 1x1/0 / 1x3/0 |
| Bypass | 700 (Ir = 1.0) | 2x350 / 2x500 | 1x1/0 / 1x3/0 |
| Output | 700 (Ir = 1.0) | 2x350 / 2x500 | 1x1/0 / 1x3/0 |
Recommended Upstream Protection and Cable Sizes for 625 kW UPS
| Maximum OCPD (A) | Cable size per phase (AWG/kcmil) Copper / Aluminum |
EGC cable size (AWG/kcmil)* Copper / Aluminum |
|
|---|---|---|---|
| Input |
1000 (Ir = 1.0) |
3x400 / 3x600 |
1x2/0 / 1x4/0 |
| Bypass |
800 (Ir= 1.0) |
2x600 / 3x400 |
1x1/0 / 1x3/0 |
| Output |
800 (Ir = 1.0) |
2x600 / 3x400 |
1x1/0 / 1x3/0 |
Recommended Upstream Protection and Cable Sizes for 750 kW UPS
| Maximum OCPD (A) | Cable size per phase (AWG/kcmil) Copper / Aluminum |
EGC cable size (AWG/kcmil)* Copper / Aluminum |
|
|---|---|---|---|
| Input |
1200 (Ir = 1.0) |
3x600 / 4x500 |
1x3/0 / 1x250 |
| Bypass |
1000 (Ir = 1.0) |
3x400 / 3x600 |
1x2/0 / 1x4/0 |
| Output |
1000 (Ir = 1.0) |
3x400 / 3x600 |
1x2/0 / 1x4/0 |
Recommended Upstream Protection and Cable Sizes for 800 kW UPS
| Maximum OCPD (A) | Cable size per phase (AWG/kcmil) Copper / Aluminum |
EGC cable size (AWG/kcmil)* Copper / Aluminum |
|
|---|---|---|---|
| Input |
1600 (Ir = 0.8) |
4x400 / 4x600 |
1x4/0 / 1x350 |
| Bypass | 1000 |
3x400 / 3x600 |
1x2/0 / 1x4/0 |
| Output | 1000 |
3x400 / 3x600 |
1x2/0 / 1x4/0 |
Recommended Upstream Protection and Cable Sizes for 1000 kW UPS
| Maximum OCPD (A) | Cable size per phase (AWG/kcmil) Copper / Aluminum |
EGC cable size (AWG/kcmil)* Copper / Aluminum |
|
|---|---|---|---|
| Input |
1600 (Ir = 1.0) |
4x600 / 5x600 |
1x4/0 / 1x350 |
| Bypass |
1600 (Ir = 0.8) |
4x400 / 4x600 |
1x4/0 / 1x350 |
| Output |
1600 (Ir = 0.8) |
4x400 / 4x600 |
1x4/0 / 1x350 |
Recommended Upstream Protection and Cable Sizes for 1100 kW UPS
| Maximum OCPD (A) | Cable size per phase (AWG/kcmil) Copper / Aluminum |
EGC cable size (AWG/kcmil)* Copper / Aluminum |
|
|---|---|---|---|
| Input |
2000 (Ir = 0.9) |
5x500 / 6x500 |
1x250 / 1x400 |
| Bypass |
1600 (Ir = 0.9) |
4x500 / 5x500 |
1x4/0 / 1x350 |
| Output |
1600 (Ir = 0.9) |
4x500 / 5x500 |
1x4/0 / 1x350 |
Recommended Upstream Protection and Cable Sizes for 1250 kW UPS
| Maximum OCPD (A) | Cable size per phase (AWG/kcmil) Copper / Aluminum |
EGC cable size (AWG/kcmil)* Copper / Aluminum |
|
|---|---|---|---|
| Input |
2000 (Ir = 1.0) |
5x600 / 6x600 |
1x250 / 1x400 |
| Bypass |
1600 (Ir = 1.0) |
4x600 / 5x600 |
1x4/0 / 1x350 |
| Output |
1600 (Ir = 1.0) |
4x600 / 5x600 |
1x4/0 / 1x350 |
Recommended Cable Sizes for Battery Cabinets
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
All wiring must comply with all applicable national and/or
electrical codes. The maximum allowable cable size is 350 kcmil.
Failure to follow these instructions will result in death or serious injury.
|
CAUTION
DANGER