990-914301A-001

Prepare the I/O Cabinet for Power Cables in Bottom Cable Entry Systems

DANGER
hazard of electric shock, explosion, or arc flash
Do not drill/punch holes for cables or conduits with the gland plates installed and do not drill/punch holes in close proximity to the UPS.
Failure to follow these instructions will result in death or serious injury.
NOTE: Cables to the external supply for Lithium-ion battery solution must be routed through the top of the I/O cabinet. Follow the procedure Prepare the I/O Cabinet for Power Cables in Top Cable Entry Systems to prepare for cables to the external supply.
NOTE: You may need to elevate the cabinet by lowering the cabinet feet or reduce the floor height directly beneath the bottom gland plates to get correct wire bending range for the power cables.
  1. Loosen the bolts and remove the gland plates in the bottom of the I/O cabinet.
  2. Drill or cut holes for cables/conduits in the bottom gland plate.
    DANGER
    hazard of electric shock, explosion, or arc flash
    Ensure that there are no sharp edges that can damage the cables.
    Failure to follow these instructions will result in death or serious injury.
    1. For bypass cables

    2. For DC cables

    3. For output cables

    4. For input cables

  3. Install conduits and install the bottom gland plates in the indicated order below the frame.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?