990-914301A-001

Route External Signal Cables to the Boards

  1. Remove the two gland plates from the top of the I/O cabinet and drill holes for the applicable Class 2/SELV (A) and non-Class 2/non-SELV (B) signal cables. Install conduits and reinstall the plates.
  2. Route the external signal cables through the cable channel and through the correct openings:
    1. Class2/SELV cables to the boards in the left door.

    2. Class2/SELV cables to the boards in the right door.

    3. Non-class 2/Non-SELV cables to the boards in the right door.

  3. Route the external signal cables to the boards in the right door:
    1. Open the right door and remove the plate from the inner door.
    2. Route the cables to the board terminals and fasten with the provided cable ties. Class 2/SELV cables (A) must be routed separated from non-Class 2/non-SELV cables (B) as shown on the illustration.
      NOTE: The external signal cables must be long enough for the door to fully open.
  4. Route the external signal cables to the boards in the left door:
    1. Open the left door and remove the plate from the inner door.
    2. Route the external signal cables to the terminals and fasten with the provided cable ties.
      NOTE: The external signal cables must be long enough for the doors to fully open.
      NOTE: Use the plate (A) for shielding of the Modbus cable.
    3. Close the door and route the PBUS cables and cables for the network management cards to the front.
      NOTE: If the input dry contact AP9810 is connected to AP9631 or AP9635CH, the total length of cables for connected equipment must not exceed 30 m (98 ft). Use the plate for shielding (A).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?