990-914301A-001

Final Mechanical Assembly of the I/O Cabinet

DANGER
hazard of electric shock, explosion, or arc flash
All panels and covers must be properly reinstalled prior to energizing the UPS.
Failure to follow these instructions will result in death or serious injury.
  1. Reinstall the cover on the door in the left side and fasten with the screws.
  2. Close the door and fasten with the screw.
  3. Reinstall the indicated cover if removed and fasten with the screws.
  4. Reinstall the cover on the door in the right side and fasten with the screws.
  5. Close the door and fasten with the screw.
  6. Reinstall the two indicated covers and close the door in the top right corner. Fasten with screws.
  7. Close the front doors.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?